Clear and re-program a pattern on the Esprit Series camera

Issue

How do I clear and re-program a pattern on the Esprit series camera?

Product Line

Pelco Cameras, Pelco Matrix

Environment

Esprit series camera 
KBD300A
KBD960

Cause

Esprit series camera doesn't save a pattern

Resolution

Clear program Pattern:

On the keyboard perform the following action:

  1. Press PRESET then 95. Camera menu appears.
  2. Tap down to "SETTINGS".  
  3. Press IRIS OPEN.
  4. Tap to "PATTERNS"
  5. Press IRIS OPEN.
  6. Tap to "CLEAR PATTERN". 
  7. Press IRIS OPEN. The pattern number you called up deleted.

Program Pattern:

On the keyboard perform the following action:

  1. Press PRESET then 95. Camera menu appears.
  2. Tap down to "SETTINGS".  
  3. Press IRIS OPEN 
  4. Tap to "PATTERNS". 
  5. Press IRIS OPEN.
  6. Tap to "PROGRAM PATTERN".
  7. Press IRIS OPEN.
  8. Move the dome to the start point.
  9. Press IRIS OPEN
  10. Move the dome to the desire pattern.
  11. Press IRIS OPEN. Pattern saved.