What power supply is recommended for the ExSite Explosionproof Camera System?

Issue

What power supply is recommended for the ExSite Explosionproof Camera System?

Product Line

Pelco Cameras

Environment

  • EHXM Series analog Explosion Proof Fixed Camera
  • IPSXM Series analog Explosion Proof Pan/Tilt Camera
  • EHXME Series IP Explosion Proof Fixed Camera
  • IPSXME Series IP Explosion Proof Pan/Tilt Camera

Cause

Request for power supply for ExSite Series Camera System.

Resolution

Pelco no longer sells a power supply for these series of cameras.

The ExSite Explosion proof camera systems requires a 120W/120VA power supply at 5 amps for the 24VAC models. 110-240VAC models can plug into any standard wall circuit.

Amp draw:

  • 100-110 VAC = 1 A
  • 240VAC = .5A
  • 24 VAC = 5 A