Can I get the DF5-PG-E1 in stainless steel with an IP66 rating?

Issue

Can I get the DF5-PG-E1 in stainless steel with an IP66 rating?

Product Line

Pelco Cameras

Environment

DF5-PG-E1

Cause

The DF5-PG-E1 made in stainless steel with an IP66 rating

Resolution

You would need to get an SMR done to get a stainless steel DF5-PG-E1 manufactured with an IP66 rating. The SMR process is started through Pelco Sales at 1-800-289-9100 or through pelcosales@schneider-electric.com.