Now that the IS20/IS21 Series Camclosure II are OBS what can I use?

Issue

Now that the IS20/IS21 Series Camclosure II are OBS what can I use?

Product Line

Pelco Cameras

Environment

  • IS20/IS21- All versions
  • FD1/FD2/FD5- All versions

Cause

A replacement for the IS20-CHV10S is needed.

Resolution

We are now selling the FD1 , FD2 and FD5 fixed dome cameras as valid replacements. Depending on the model of  IS20/IS21 Series Camclosure II you currently have, there will be a need to choose the correct replacement from the FD1, FD2 or FD5 series of cameras.