Is it possible to access the value of a doors ADA output for programming or reporting via graphics, listviews or reports?

Issue

Is there a way to display the value of a doors ADA output or to use this value in a Plain English program?

Product Line

Andover Continuum

Environment

ADA output

Door attributes

Cause

Need to display and track the value of a doors ADA output.

Resolution

There is no sanctioned way to access or use the value of a doors ADA output.  While in some cases it may be possible to create a separate output object with the same channel number to track this value, this kind of configuration is known to have issues and it is not recommended.