What is the power requirement for the IS20/IS21 Series Cam closure 2 indoor dome system?

Issue

What is the power requirement for the IS20/IS21 Series Cam closure 2 indoor dome system?

Product Line

Pelco Cameras

Environment

IS20/IS21- All versions

Cause

Customer wanted to make sure he has the correct power supply for the IS21-DNV10F.

Resolution

The power requirement for the IS20/IS21 Cam Closure 2 indoor dome System is as follows:

  • NTSC: 24 VAC, 60 Hz or 12 VDC, 280 mA
  • PAL: 24 VAC, 50 Hz or 12 VDC, 280 mA .