Is the VA6100 Series or VA6200 Series Sequential Video Switcher with Alarm still available?

Issue

Is the VA6100 Series or VA6200 Series Sequential Video Switcher with Alarm still available?

Product Line

Pelco Video Management

Environment

  • VA6100 Series Sequential Switcher
  • VA6200 Series Sequential Switcher

Cause

Request for VA6100 or VA6200 Series Sequential Switcher.

Resolution

The VA6100 Series or VA6200 Series Sequential Video Switchers are no longer available for sale. 

 

However, these units can be returned to Pelco for repair if they are damaged.