Can I use the IRD2024 to control a Spectra IV Se Series Dome?

Issue

Can I use the IRD2024 to control a Spectra IV Se Series Dome?

Product Line

Pelco Cameras

Environment

Spectra IV SE- All versions

Cause

Customer wanted to control the SD429-F1 using the IRD2024.

Resolution

The IRD2024 Receiver/Driver is not needed to control the Spectra IV series cameras. The Spectra IV SE series cameras have a receiver board built into them.