ERD97P21-U voltage selection jumper part numbers.

Issue

What are the part numbers for the jumpers that come with the ERD97P21-U?

Product Line

Pelco Cameras, Pelco Transmission & Power

Environment

ERD97P21-U

Cause

Replacement jumpers for the 24VAC Pan and tilt are needed.

Resolution

Here is a list of the jumper plugs that are shipped with the ERD97P21-U:

  • CON10J001ASSY = PLUG,WIRING,RX/DX,PAN/TILT POWR,24V
  • CON10J002ASSY = PLUG,WIRNG,RX/DX,PN/TLT PWR 120/230
  • CON10J003ASSY = PLUG,WIRING,RX/DX,CAMERA POWER,24V
  • CON10J004ASSY = PLUG,WIRING,RX/DX,CMRA PWR,120/230V
  • CON10J005ASSY = PLUG,WIRING,RX/DX,INPUT PWR 24V
  • CON10J006ASSY = PLUG,WIRING,RX/DX,INPUT POWER,120V
  • CON10J007ASSY = PLUG,WIRING,RX/DX,INPUT POWER,230V

Click HERE for power connections on the ERD97P21-U