Does the EH14-2 come with a 24 VAC power supply?

WARNING

ELECTROSTATIC DISCHARGE REQUIRED.
Discharge all static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.

Issue

Does the EH14-2 come with a 24 VAC power supply?

Product Line

Other, Pelco Cameras

Environment

  • EH14-2

Cause

EH14-2 Enclosure is not powering a camera.

Resolution

The EH14-2 Enclosure is designed to utilize 24 VAC in order to power the heater and blower, as well as provide a 24 VAC output in order to power a camera. 

This enclosure will require a 24 VAC power supply that can supply a minimum of 30 Watts. This will power both the enclosure and the camera.