What is the part number for the side covers of an ESPT31 Esprit?

WARNING

ELECTROSTATIC DISCHARGE REQUIRED.
Discharge all static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.

Issue

What is the part number for the side covers of an ESPT31 Esprit?

Product Line

Pelco Cameras

Environment

  • ESPT31

Cause

Customer request to replace the outer side covers of an ESPT31 Esprit due to wear and tear or damage.

Resolution

  • MF80-9042-002C Side Cover with Conduit Plug Hole
  • MF80-9042-001C Side Cover
  • MF80-4252-120C Conduit Plug
  • ZH69-0204-1197 O-Ring for Conduit Plug