Issue
Can I use the IPCT01 to replace the IPS-RMK?
Product Line
Pelco Cameras
Environment
- IPCT01
- IPS-RMK
Cause
Customer is looking to use the IPCT01 in place of the IPS-RMK.
Resolution
The IPCT01 is designed for Sarix IP Enhanced (IxE) and Sarix Professional (IxP) series cameras ONLY whereas the IPS-RMK only worked with the Spectra IV and Spectra III analog cameras.