How do I get into the menu of a Spectra Series camera using the Avigilon Software?

Issue

How do I get into the menu of a Spectra Series camera using the Avigilon Software?

Product Line

Pelco Cameras

Environment

  • Spectra III Series
  • Spectra IV Series
  • Avigilon

Cause

Spectra Series cameras in use with the Avigilon software system.

Resolution

  1. Select the camera you wish to program.
  2. Ensure that the camera selected is in full screen mode.
  3. Select the Person icon in the lower left corner of the screen.
  4. Select the OSD option.
  5. Use the Iris Open button to enter the OSD menu.