Issue
Thermistor temperature readings are 10-20°F below actual temperature
Environment
I/NET Site
Cause
Thermistor temperature readings are 10-20°F below actual temperature
Resolution
One of the universal inputs on this controller is using a 4-20ma sensor whose resistor input configuration has a 10K ohm in the B-slot instead of a 249 ohm in the A-slot.