Is there a pipe extension for the Spectra Series Pendant Mount Domes?

Issue

Is there a pipe extension for the Spectra Series Pendant Mount Domes?

Product Line

Pelco Cameras

Environment

  • Spectra III Series Cameras
  • Spectra IV Series Cameras
  • SP01-146A
  • SP01-146B

Cause

Request to mount a Spectra Series Pendant camera with a pipe extension.

Resolution

Pelco offers two 1 1/2 inch NPT Pipe extensions.

  • SP01-146A, 12 inch Pipe Extension
  • SP01-146B, 40 inch Pipe Extension

Note: MRCA is a ceiling mount designed for use with SP01-146A and SP01-146B extension pipes