Issue
Is the FMCI-AF1MM1STM (Mini-Transmitter) compatible with the FMCI-BF1MM1ST (Standard Receiver)?
Product Line
Pelco Cameras, Pelco Video Management
Environment
- FMCI-AF1MM1STM
- FMCI-BF1MM1ST
- USRACK
Cause
Requirement to use a Mini-Size Fiber Transmitter and have a Standard Size Receiver at the head end; so that a rack (USRACK) can be used.
Resolution
As long as the same transmission distance model is selected with both the transmitter and the receiver, you can use a combination of mini and standard size transmitters and receivers.
For example, these two models are compatible with each other, even though they are different sizes.
Transmitter model
- FMCI-AF1MM1STM
Receiver model
- FMCI-BF1MM1ST