Unable to program a port address into a CM6800 when using Coaxitron for PTZ control.

Issue

Unable to program a port address into a CM6800 when using Coaxitron for PTZ control.

Product Line

Pelco Matrix

Environment

  • CM6700 Series
  • CM6800 Series

Cause

When programming a CM6800 for PTZ control, there is no ability to enter a port address for the camera.

Resolution

When using coaxitron to control a PTZ camera, the address of the camera will match the port number that it is plugged into on the matrix.

For Example:

A camera plugged into input 4 of a CM6800 will have the address of 4.