Can you adjust the speed of the pan and tilt with the MPT9000?

Issue

Can you adjust the speed of the pan and tilt with the MPT9000?

Product Line

Pelco Cameras, Pelco Matrix

Environment

  • KBD9000
  • MPT9000CZ
  • MPT9000PZ

Cause

Customer has a camera that is moving fast when using the MPT9000.

Resolution

The MPT9000 is a 15-bit Coaxitron and it will NOT allow you to adjust the Pan, Tilt, nor Zoom speed. If you need the speed adjustment you will have to use a Matrix with the KBD300A or KBD200A and a Coaxitron translator that outputs 32-bit Coaxitron instead.