PMM9A replacement monitor.

Issue

  • What can I replace my PMM9A with?
  • What does Pelco offer as a direct replacement to my PMM9A?
  • The PMM9A went dead and I need a replacement model number for it.

Product Line

Pelco Monitors

Environment

PMM9A

Cause

The PMM9A is so old, there are no longer references towards this type of monitor.

Resolution

The PMM9A was a 9" CRT screen that was a black/white screen. Since this monitor is so completely obsolete, there is nothing that will be a direct replacement, or, even a close replacement as everything has moved over to the flat panel monitors.