Can I power the Sarix IM10LW or IMS0LW series IP mini Domes with Sure Vision with 24 AC?

Issue

Can I power the Sarix IM10LW or IMS0LW series IP mini Domes with Sure Vision with 24 AC?

Product Line

Pelco Cameras

Environment

IMS0LW10-1 IM10LW10-1 IM10LW10-B1

Cause

Customer wanted to power the IM10LW10-1 with 24 VAC.

Resolution

The Sarix IM10LW and IMS0LW IP mini domes are Power over Ethernet (PoE) only and therefore, you cannot use 24VAC for powering these cameras.