Can a Fixed Speed Coaxitron Controller adjust the zoom lens on the ExSite Fixed Explosion Proof Camera Series?

Issue

Can a Fixed Speed Coaxitron Controller adjust the zoom lens on the ExSite Fixed Explosion Proof Camera Series?

Product Line

Pelco Cameras

Environment

  • KBD9000
  • MPT9000
  • EHXM Series ExSite Explosion Proof Camera System

Cause

Request to control the zoom lens on a Fixed ExSite Series camera using a Coaxitron Controller.

Resolution

The lens of the Fixed ExSite Series Explosionproof Cameras can be controlled by using a Fixed Speed Coaxitron Controller. Compatible controllers include:

  • KBD9000
  • MPT9000CZ
  • MPT9000PZ