EH14 heater and blower

Issue

Can you order the EH14 then add the heater and blower to make it the EH14-2 or EH14-3?

Product Line

Pelco Cameras

Environment

  • EH14
  • EH14-2
  • EH14-3

Cause

Adding a heater or blower to a EH14

Resolution

There is no heater or blower kit for the EH14

If a heater and blower is required Order EH14-2 for 24 VAC or EH14-3 for 230 VAC