Can a VGA monitor be used on a CM6800 matrix System?

Issue

Can I use a monitor that only has a VGA input on the CM6800 matrix System?

Product Line

Pelco Monitors, Pelco Matrix

Environment

CM6800 Matrix

Cause

Connecting a Monitor that only has a VGA input. 

Resolution

The CM6800 Matrix Switcher is BNC output only.

Note: Pelco does not recommend the use of a third party BNC to VGA converter, as it may degrade the video signal.