Motion detection configuration for Sarix IBP or IMP Professional line of cameras through Endura Workstation.

Issue

Motion detection configuration for Sarix Professional series IP cameras using the Endura workstation.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Endura VMS
  • Sarix IBP or IMP series IP cameras

Cause

New Sarix Professional series IP cameras have been added to an Endura network where recording via motion detection is preferred.

Resolution

Please refer to the knowledge base article titled "Configuring Motion and Motion Recording in the WS5000 Software," but note the following exceptions:

  1. Only one motion detection zone is supported (Zone 1).
  2. The motion detection zone must be rectangular- or square-shaped
  3. There are three sensitivity levels supported in the camera, "High," "Medium," and "Low" they correlate as follows:
    1. 0 - 32 = Low
    2. 33-65 = Medium
    3. 66 to 100 = High
  4. The threshold blocks or percentage has no effect on overall camera sensitivity.

Refer to the following screenshot as an example: