USRACK power input

Issue

Can the USRACK be powered with 230 VAC / 60Hz power?

Product Line

Pelco Transmission & Power

Environment

  • USRACK
  • 230 VAC Power

Cause

Will the USRACK support 230VAC.

Resolution

USRACK input power ranges from 90 to 264 VAC at 70W maximum

Click here for spec sheet