What Fiber Transmitter and Receiver can replace the FT8304 and FR8304 Series?

Issue

What Fiber Transmitter and Receiver can replace the FT8304 and FR8304 Series?

Product Line

Pelco Transmission & Power

Environment

  • FT8304 Series Fiber Transmitter
  • FR8304 Series Fiber Receiver
  • FTV40 Series Fiber Transmitter
  • FRV40 Series Fiber Receiver

Cause

Request to purchase the FT8304 and FR8304 Series Fiber units which are no longer produced.

Resolution

The replacement model for the FT8304 and FR8304 Series Fiber Transmitter and Receiver will be the FTV40 and the FRV40 Series Fiber Transmitter and Receiver. The specification sheet for this series can be found at the following link.

FTV40/FRV40 Fiber Transmitter and Receiver