What Fiber Transmitter and Receiver can replace the FT8301A and FR8301?

Issue

What Fiber Transmitter and Receiver can replace the FT8301A and FR8301?

Product Line

Pelco Transmission & Power

Environment

  • FT8301 Series Fiber Transmitter
  • FR8301 Series Fiber Receiver
  • FTV10 Series Fiber Transmitter
  • FRV20 Series Fiber Receiver

Cause

Request to purchase FT8301AMSTR and FR8301MSTR. These products are no longer being produced.

Resolution

The replacement Fiber Transmitter and Receiver units for the FT8301A and FR8301A will be the FTV10 and FRV20 Series Fiber units. The specification sheet for these series can be found at the following link.

FTV10 Series

FRV20 Series

Note: Due to different component assembly the RACK will also have to be replaced:

USRACK