How to adjust the record settings on the DX4000.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Select the size or resolution at which video is recorded, the recording rate (frames per second), and image quality for recording video on each camera that is attached to the DX4000.

Product Line

Pelco Video Management

Environment

DX4000 Series DVR all versions

Cause

Installation and Maintenance.

Resolution

Press Menu on the front panel of the DX4000: Opens the system menus. Login as Administrator

  • Use the Control buttons to Navigate through menu options.
  • Return: Cancels a setup operation or returns you to a previous menu or mode.
  • Enter: Applies any changes that you enter and accesses selected menus.

 

Use the Record menu to select the size and quality of recordings, to set up recording schedules, and to set up alarm-based recording.

 

  • Size/Record Rate/Quality: Select the size or resolution at which video is recorded, the recording rate (frames per second), and image quality for recording video on each camera that is attached to the DX4000.  
  • Timer Recording Setup: Use this option to set up a recording schedule and to set up motion detection.
  • Alarm Recording Setup: Use this option to set up recording based on alarms.