At what temperature does the fan and heater of the EH4700 Series Enclosures activate?

Issue

At what temperature does the fan and heater of the EH4700 Series Enclosures activate?

Product Line

Pelco Cameras

Environment

  • EH4718 -1/-2/-3
  • EH4722 -1/-2/-3

Cause

Verification on if a fan or heater should be currently activated based on current environmental conditions.

Resolution

The fan of the EH4700 Series Enclosure is set to activate between an internal temperature of 77° F  and 93° F and will remain on until the internal temperature reaches somewhere between 62° F and 78° F.

The heater of the EH4700 Series Enclosure is set to activate between an internal temperature of 42° F  and 58° F and will remain on until the internal temperature reaches somewhere between 72° F and 88° F.