Does the LCM driver support tunneling?

Issue

Does the LCM driver support tunneling?

Product Line

TAC I/A Series

Environment

R2 UNC with LCM driver

Cause

Tunneling is needed to make programming changes to the LCM's.

Resolution

Yes, it is possible to tunnel through the UNC to the LCM's, but it requires an RS-232 connection from the UNC to one of the LCM's.  See the LCM Integration Guide F-27422-2 for details.