Can the ExSite IP Series Explosion Proof Camera System be powered by Power Over Ethernet?

Issue

Can the ExSite IP Series Explosion Proof Camera System be powered by Power Over Ethernet?

Product Line

Pelco Cameras

Environment

  • EHXME IP Series Fixed ExSite Explosionproof Camera 
  • IPSXME IP Series PTZ ExSite Explosionproof Camera

Cause

Request to power an ExSite IP Series Camera with PoE.

Resolution

The ExSite IP Series Explosionproof cameras all require either a 24 VAC or 100 to 240 VAC power supply. These cameras are not compatible with Power over Ethernet.