Is there a shortcut key to call up cameras by number in the WS5000 program?

Issue

The user wishes to call up cameras using the keyboard instead of right-clicking on the video and choosing Select Camera by Number...

Product Line

Pelco Video Management

Environment

WS5000 Advanced System Software, all versions
WS5200 Advanced System Software, all versions

Cause

It is faster for some people to use keyboard shortcuts (hot keys) than the mouse.

Resolution

The keyboard shortcut to call up a camera by number is F4.