Discontinuation of HID SmartTOUCH Fingerprint readers

Issue

HID Biometric reader product obsolescence.

Product Line

TAC I/NET, Andover Continuum, Field Devices

Environment

HID Desfire and Mifare Smart card and Fingerprint readers.

As used on Continuum and I/Net Access Control.

Cause

HID have discontinued these readers.

Resolution

HID have discontinued production of their SmartTOUCH SB10 and SBK10 Desfire and Mifare fingerprint readers.

Part numbers affected are:

HID Ref: 800-8052, SE P/N 654 1903 000 - SB10 Desfire Fingerprint reader.

HID Ref: 800-8057, SE P/N 654 1904 000 - SBK10 Desfire Fingerprint reader with keypad.

HID Ref: 800-8050, SE P/N 654 1901 000 - SB10 Mifare Fingerprint reader.

HID Ref: 800-8055, SE P/N 654 1902 000 - SBK10 Mifare Fingerprint reader with keypad.