Configuring a static IP address to WS5070 or Windows 7 server.

Issue

The customer is using static IP addresses instead of DHCP.

Product Line

Other, Pelco Video Management

Environment

Endura WS5000/WS5200 or Windows 7 platform

Cause

The customer wants to assign a static IP address to the workstation because the rest of the Endura devices are configured with a static IP address and the system manager is not configured to be a DHCP server.

Resolution

Sign into the Workstation with administrative credentials and follow the instructions at the web site below.

 

Setting a Static IP Address in Windows 7