What is a replacement camera for the (obsolete) Camclosure 2 Series IS20/21 and IS50/51 camera models?

Issue

Replacement model is needed for obsolete Camclosure 2 Series IS Camera Models.

Product Line

Pelco Cameras

Environment

Camclosure 2 Series Camera Models:

  • IS20/21
  • IS50/51

Cause

Camclosure 2 Series Camera Models IS20/21 and IS50/51 are obsolete.

Resolution

The replacement cameras for the obsolete Camclosure 2 Series IS camera models are the new FD Series camera models.

  • IS20/21 camera models can be replaced with the FD1 or FD2 Series camera models.
  • IS50/51 can be replaced with the FD5 Series camera model.