Cyrillic character - Vista has no support for Unicode


  • Do not get any values in webstation
  • Bindings in TGML do not work

Product Line

TAC Vista


  • Vista
  • Cyrillic


If bindings in TGML contain Cyrillic characters and the operating system installed is set to a language that can not handle Cyrillic (i.e English), the bindings will not show their values.


  1. Set the region and language settings all to the desired language, i.e Russian or Polish.
  2. Be sure Webstation is set to handle the language by installing the correct language pack.
  3. Edit the TGML and make a small change so you can save again, this time the Cyrillic letters will be understood by Tacos.