Error during installation of OpenLNS Server on Windows 8.1 x64

Issue

On rare occasions you will get an error during the installation of Echelon OpenLNS Server on Windows 8.1 64 bit saying that the installer can't create specific registry keys.

Product Line

TAC Vista, SmartStruxure Solution, Other

Environment

OpenLNS

Windows 8.1 64 bit

Cause

For some reason the user doesn't have the appropriate permissions to access those registry keys

Resolution

Add the registry keys manually and run the installer again.

You can also run this reg file that will add the keys