Does Pelco charge a fee to add IP cameras to an Endura system?

Issue

Many other video-management systems charge a fee to connect IP cameras to a system.

Product Line

Pelco Cameras, Pelco Video Management

Environment

Endura video management system

Cause

Not applicable.

Resolution

There is no charge to add a Pelco IP camera or encoder to an Endura system. Pelco IP cameras and encoders are detected automatically and register themselves once connected to the network.

Third-party cameras require the use of a UDI5000-CAM.

Analog cameras must be connected to an IP encoder, such as the NET5500T, to work in Endura.