Will I be able to ping the Spectra IV IP without the Dome Drive connected to the Back Box?

Issue

Does the Spectra IV Ip sub assemblies has stand alone functions?

Product Line

Pelco Cameras

Environment

  • Spectra IV IP MPEG4
  • Spectra IV IP H.264

Cause

Installation and Service

Resolution

The spectra IV IP assemblies must be connected for the camera to connect to a network:

  1. Connect the Dome Drive to the swivel down back box Door Assembly.
  2. Power on the camera.
  3. Connect and link the camera to a network.