No video with a Sarix Professional IP camera when using ONVIF communication.


Configuring a Digital Sentry recorder to record video from a Sarix Professional IP camera using the ONVIF driver results in No Video.  No Video in both DS ControlPoint and DS Admin.

Product Line

Pelco Cameras, Pelco Video Management


  • Digital Sentry 7.6.32
  • DS NVs
  • Sarix Professional Series v03.29.21 and below
    • IBP
    • IMP
    • IXP


The Secondary Stream in the Sarix Pro IP cameras web interface is cleared and does not have any values.


With software versions 03.29.21 and below, if the secondary video stream is cleared, ONVIF communication will fail resulting in video loss in Digital Sentry or other VMS software.  Upgrade to firmware 03.29.27 and above to resolve.

Verify the following knowledge base article has been followed: How do I add an ONVIF compatible IP camera to a Digital Sentry system?