Error: Failed to replace dbexporter when installing ES 1.5

Issue

Error: Failed to replace dbexporter when installing ES 1.5.

The error appears when files are being copied to machine.

Product Line

SmartStruxure Solution

Environment

ES

Cause

Other instance of ES running.

Resolution

Go in Control Panel\Administrative Tools\Services and make sure there is no Enterprise Server service running.