Spectra IV Spring Paddle part number for In-Ceiling back boxes.

Issue

  • We lost our holders for the Spectra back box; what is the part number?
  • What is the part number for the Spring Paddles for the Spectra IV cameras?
  • There are two side ears that are on the BB4-F and we need the part number for them.

Product Line

Pelco Cameras

Environment

BB4-F

Cause

The customer needed to know the part number for the Spring Paddles on the side of the BB4-F.

Resolution

The part number for the Spring Paddle parts on the side of the BB4-F is 70610027. The Spring Paddles look like this:

BB4-F side paddle part number