Video connections on CM6700

Issue

Where to connect cameras on CM6700

Product Line

Pelco Cameras, Pelco Matrix

Environment

  • CM6700
  • Video cameras
  • Video inputs

Cause

No video or PTZ control

Resolution

Plug camera into one of the available ports on the back of the CM6700

  • Odd number sequence on top row
  • Even number sequence on bottom row