PT280 series Pan/Tilt unit torque ratings.

Issue

What is the torque for the PT280 Pan/Tilt unit?

Product Line

Pelco Cameras

Environment

PT280-24P, PT280P

Cause

Customer had pre-sales inquires about the torque specifications as this value is NOT on the Spec Sheet.

Resolution

The PT280 series Pan/Tilt units has the following torque ratings:

  • Pan: 80 in-lbs @ 24VAC 60Hz (drive gear limited)
  • Tilt: 80 in-lbs @ 24VAC 60Hz input