What is the part number for the terminal plugs on the CM9760-CDU-T?

Issue

What is the part number for the terminal plugs on the CM9760-CDU-T?

Product Line

Pelco Video Management, Pelco Matrix

Environment

  • CM9760-CDU-T

Cause

Request for part numbers to replace the removable screw terminals for the CM9760-CDU-T.

Resolution

  • The part number for the three position plugs used for the camera outputs of the CM9760-CDU-T is TB05-9105-0803G.
     
  • The part number for the two position plug used for the control signal input of the CM9760-CDU-T is TB05-8103-1202G.