Dip switch settings for the Sarix TI Series Thermal IP Positioning System.

Issue

What are the dip switch settings for communication protocol, address, and baud-rate on the Sarix TI Series Thermal IP Positioning System?

Product Line

Pelco Cameras

Environment


Sarix TI Series Thermal IP Positioning System

Cause

Installation & Configuration

Resolution

SW1 = Set the baud rate
SW2 = Set receiver address

Click HERE for the addressing table on page 78 to 80