IEC Connector types for Pelco monitors.

Issue

  • What plug style do Pelco monitors use?
  • I am needing to order some power plugs for my Pelco monitors and I need to know what is the coupler/coupling style of the cords that are used?
  • What are the coupler styles in use on the Pelco monitors?
  • What are the IEC couplers for the Pelco monitors?

Product Line

Pelco Monitors

Environment

PMCL series monitors.

  • PMCL500A and PMCL500F series
  • PMCL500HB
  • PMCL500NB
  • PMCL400NB
  • PMCL300A, PMCL300F

Cause

Customers need to know what the plug style is for their power cords.

Resolution

Most ALL of Pelco's Flat panel PMCLx00xx series monitors will have either the C13 (Female side - plugging into) or C14 (Male side - receiving) plug couplers/coupling styles DIRECTLY on the back of the monitors themselves. However, some of the power cords, after plugging into the monitor itself, requires the use of a power box/transformer in between the monitor and the Mains power source and therefore the cord itself also terminates into the C7P (Female side)/C8P (Male side). For reference to the images to the plugs themselves, please see the IEC 60320 article.