How can you convert an analog camera signal to an IP addressed camera?

Issue

How can you convert an analog camera signal to an IP addressed camera?

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Any Analog based camera signal
  • NET5400T Series Encoders
  • NET5500 Series Video Encoders

Cause

Requirement to convert an analog camera to an IP based signal.

Resolution

The NET5400T Series Encoder has the ability to convert an analog signal to an IP address that can be viewed over a network. 

More information can be found regarding the NET5400T Series on its Specification Sheet.

 

The NET5500 Series is a high performance, single-chanel to multi-chanel video encoder that integrates analog cameras into an IP video signal.
NOTE: Due to the hardware limitation of the existing design, Pelco recommnends limiting the number of PTZs connected to a NET5500.

NET5500 Series Encoder PTZ Limitations.