How can I provide power to a 24VAC camera mounted inside a 120 VAC EH4700 Enclosure?

Issue

How to power opposing devices that require different voltages?

Product Line

Pelco Cameras

Environment

  • EH4718-1 EH4722-1 O/I-OUTLET

Cause

  • Sales and Installation Support
  • Customer wanted to power a 24 VAC camera in the EH4718-1.

Resolution

Use the O/I-OUTLET and the TF2000 to power a 24 VAC camera with a EH4700 Series Enclosure that has 120 VAC power.