How to setup the static IP Address of the IPCT01 Camera Tester and IP Camera's IP Address

Issue

How to setup the IP Address of the IPCT01 Camera Tester and IP Camera's IP Address

Product Line

Field Devices, Other, Pelco Cameras, Pelco Transmission & Power

Environment

  • IPCT01 "Tester"
  • Sarix IL, IXP, IBP, IMP, IXE, IME
  • ONVIF*

Cause

Setup the IP Address of the IPCT01 Camera Tester and IP Camera's IP Address

Resolution

1.  Press Setup icon on the Main Menu
2. Press Setup-IP icon
3. Press Setup-IP Connection icon

Setup Tester IP Address:

1. Select TESTER Address field, open Keyboard pad to enter the ip address
2. Press SET button to save TESTER IP Address

Setup Camera IP Address:

1. Select Camera IP field, open keyboard pad to enter the ip address
2. Press Check Box to save the Camera IP Address
3. Press Green Check button on the lower right hand corner to exit out.

 

*ONVIF requires optional license IPCTO1-EN-ONVIF